This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CD4047B: the unique operation of the monostable multivibrator and retrigger randomness

Part Number: CD4047B
Hi,
I'm trying to run the chip using the cd4047 chip in monostable mode with time extension on demand. The designed time tM = 2.48 RtCt is approx. 38 sec. (ceramic 30uF and 510kOhm). 12V power supply filtered with 100uF / 25V capacitor. I made the test on 2 copies - the same problem occured. I am sending an oscillogram of signals on individual pins of the system.
I am asking for help in finding the cause. Please provide more detailed information about the operation of the system and design recommendations. Best regards
  • Hi,

    The data sheet has all the info needed to set up this device. First thing I recommend is to check all of the control signals to make sure they are at the right levels. Then I would check to make sure you are meeting the timing requirements in the Dynamic Electrical Characteristics.

    It would help to see a time scale for the scope shot. It would be good to also zoom in around the pulse giving issues.

  • Thanks for quick replay. The time base is visible on the picture - 25.0 sek/div. Driving signals are beeing delivered from outputs of standard cmos circuit (cd4093)

  • Hi,

    Thanks for those details, were you able to perform all of the other checks I recommended?

    Also, are pins 8 and 12 tied together? 

  • Hi, As You can see on the oscillogram: pins 8 and 12 are marked as tied together, and they are tied indeed. The problem is that retrigger execution is randomness. I really don't know if it is possible to execute it any state of the system, what happens if i give multiple retrigger pulses one after the other while timing  (datasheet does not mention about that!). The other problem is that I noticed about twice for a long time (see oscillogram - changes in the state of oscillator output). Why the system does not guarantee repeatability of operation?

  • Hi, again.

    In addition to my thoughts - Fig.8 Retrigger mode waveforms, from 4047 datasheet.

  • Hi,

    You basically recreated the example to the right of that waveform and in that scenario the retriggering should be happening. Unfortunately, due to the age and it being a part acquired by Harris, support for this part will be limited. I still recommend zooming in on the pulse that is being ignored to see in a smaller time scale if anything is visible. 

  • Hi,

    my example of pulse no 2 is not exactly like the one on the right - I was trying to explain my doubt about the situation when the retriggering pulse is comming during the change of oscillator output level. I am constantly investigating whether the retrigger pulse can come at any point in the system state because of retrigger randomness. At the moment I am abandoning this project with cd4047 and redesigning it with a different chip. Thank you for your comments.