This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXB0106: Is Port A 5V tolerant ?

Part Number: TXB0106


Hi,

Is Port A 5V tolerant?
"Recommended Operating Conditions" denies Port A's 5V tolerance, but "Absolute Maximum Ratings" has VI = 6.5Vmax, so 5V input is allowed.
If doesn't have 5V tolerant, I think the VI (Port A)depends on Vcca.

When the customer's circuit is Vcca = 3.3V, 5V may be input to Port A. Please tell me if it works safely.

Best regards,
Hiroshi