This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Auto sensing Level Translators supports 1.2V to 5.5V I/O

Other Parts Discussed in Thread: LSF0108

Hi,

We need 8 channel Level translator with Auto direction sensing feature for GPIOs (I/O supply : 1.2V to 5.5V).

Requirement:
1) In our design, A side will be in fixed 3.3V supply & B side has to be changed from 1.2V to 5.5V.
2) Signals will translate from A to B & B to A using auto direction sensing feature.
3) There should not be any condition such that VCCA<VCCB or VCCB<VCCA.

Please provide the IC that suffices the above requirements.

Thanks

Ahamed Faize

  • The only device that can support this is the LSF0108. Vref_A must be connected to the lowest possible supply voltage (1.2 V), the resistor at Vref_B to a higher voltage; the voltages at the I/O pins and their pull-up resistors are independent from the reference voltages.

  • Thanks for the quick response.

    In  LSF0108, always VrefA voltage has to be lower than VrefB for proper operation. 

    But in our our case. the conditions like VrefA>VrefB or VrefB>VrefA should not be there so that we can translate from 3.3V level on A side to any other levels(less than or greater than 3.3V) on Bside.

    So this part will not suffice the design considerations.

    Thanks

    Ahamed Faize

  • As I said, Vref_A/Vref_B are independent from the signal voltages.

  • Hey Ahamed,

    This will be the only device that can work here. I recommend watching these training videos on the LSF family to better understand what Clemens means here.

  • Thanks. I will see the video.

    Just please confirm the below understanding :

    1) In A side the I/O line voltage can go maximum up to Vref_A & in B side the I/O line voltage can go maximum up to Vref_B.

    2) If the above is true, I/O line voltage on A side has to be lower than B side

    Regards,

    Ahamed Faize

  • On the A side, the I/O line voltage can be higher than Vref_A.
    On the B side, the I/O line voltage can be lower or higher than Vref_B.

    The only restrictions are that Vref_A < Vref_B, and that no voltage is lower than Vref_A.

  • Hi team,

    After going through the datasheet. I concluded the below major points.

    1) We can use this translator for translating multi voltage level(1.2V to 5.5V) at A side to multi voltage level(1.2V to 5.5V) at B side or vice versa.

    2) But for Using this translator for GPIO application as push pull configuration

                      - We have to fix the direction A to B or B to A. 

                      - For A to B translation, Pull up resistor has to be put on B side. For B to A translation, Pull up resistor is not needed. (Refer Figure 8 in LSF0108 datasheet)

                      - So It will not support Bidirectional communication for GPIOs.

    Please confirm the above. If it is true, we can't use this translator. Because we need the translator with push pull configuration, Auto-Direction Sensing, multi level voltage translation (1.2V to 5.5V at any side).

    Kindly provide your suggestion.

    Thanks,

    Ahamed Faize

  • The LSF passes low voltages, and relies on the pull-up resistors to generate high voltages. This indeed means that all LSF outputs are open-drain outputs.

    In general, the LSF does support bidirectional communication with GPIOs. Why are open-drain signals a problem in your case?