This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXS0104E: about one of VCCA and VCCB is not powered up, will it damage device?

Part Number: TXS0104E

Hi Dear expert,

My customer has a question regarding to TXS0104E, they have one application scenario that VCCA or VCCB is not present, only one supply is on, will it damage the device?

I checked the datasheet, quote below:

"The TXS0104E device does not require power sequencing between VCCA and VCCB during power-up so the power-supply rails can be ramped in any order. A VCCA value greater than or equal to VCCB (VCCA ≥ VCCB) does not damage the device, but during operation, VCCA must be less than or equal to VCCB (VCCA ≤ VCCB) at all times. The output-enable (OE) input circuit is designed so that it is supplied by VCCA and when the (OE) input is low, all outputs are placed in the high-impedance state. To ensure the high-impedance state of the outputs during power up or power down, the OE input pin must be tied to GND through a pulldown resistor and must not be enabled until VCCA and VCCB are fully ramped and stable. The minimum value of the pulldown resistor to ground is determined by the current-sourcing capability of the driver."

So should be ok, right? Looking forward to your reply.

BR, Joyce