This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXS0108E: TXS0108E

Part Number: TXS0108E

Hello. 

The component TXS0108EPWR, can be used to make USB pin connection (5V) to pins of a microcontroller (1.8V).

The microcontroller uses the pins at 1.8V and I want to connect DM, DP and USB_DET, to have communication and debug.

If I could use it? Or is there some other component that I can use.

And if so, there will be a TXS0108EPWR with fewer inputs.

Thank you.

Regards.