Part Number: TXB0106
HI Expert,
Regarding Pin models in TXB0106 IBIS model
TXB0106_IO_B_33 3.3 volt Vcc
TXB0106_IO_B_OS_33 3.3 volt Vcc
What is difference for above pin models?
Thanks
Muk
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TXB0106
HI Expert,
Regarding Pin models in TXB0106 IBIS model
TXB0106_IO_B_33 3.3 volt Vcc
TXB0106_IO_B_OS_33 3.3 volt Vcc
What is difference for above pin models?
Thanks
Muk
Hi Mukuno-san,
From the IBIS model file of the TXB0106:
IBIS 3.2 SYNTAX CANNOT DESCRIBE THE CHARACTERISTICS OF
ANY OUTPUT STRUCTURES THAT DYNAMICALLY CHANGES THE
IMPEDANCES DURING THE TRANSITION. THIS DEVICE USE SIMILAR
OUTPUT STRUCTURE AND THEREFORE THE SIMULATION RESULTS
MAY NOT BE ACCURATE. TI RECOMMENDS THE USE OF SPICE
SIMULATION WHEN SIMULATION ACCURACY IS IMPORTANT.
This device includes a one-shot circuit at the output of each pin (OS) that increases the drive strength for a short period of time (~30ns). This is represented by the "OS" model, while the other model represents the static model. These two can be used in parallel to more accurately represent the output of the device, however the difference in the edges is minimal from just using the OS model -- I would recommend to do any type of signal integrity analysis with the OS model set to a 30ns pulse width.