Part Number: SN74AVC2T245
Other Parts Discussed in Thread: SN74AXC2T245, SN74AXC2T45
Hi team,
I just want to confirm that whether customer can use SN74AVC2T245 as buffer for SIM card application. Please advised. thanks!
Best Regards,
Leroy Song
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN74AVC2T245
Other Parts Discussed in Thread: SN74AXC2T245, SN74AXC2T45
Hi team,
I just want to confirm that whether customer can use SN74AVC2T245 as buffer for SIM card application. Please advised. thanks!
Best Regards,
Leroy Song
The speed is 4MHz and signals are clock data and reset.
Best Regards,
Leroy Song
The data line is bidirectional, so the AVC will not work.
TI makes SIM level translators.
Hey Leroy,
This is a generic translator and does not care what communication interface its being used for. If the parameters listed in the data sheet meet the system parameters then it can work. However, I recommend the customer use the newer SN74AXC2T245.
Also just note this is a 2 channel device and it looks like you mentioned 3 different signals.
Dylan,
Thanks for the comment. Here are some follow-up questions.
) mentioned about SN74AXC2T45 can be used for Clock and Reset, so can I use SN74AXC2T245 for data and SN74AXC2T45 for the other two signals (Clock and reset)? What is the difference between these two parts?Best Regards,
Leroy Song
The different between the '45 and the '245 device is that the '245 has two separate DIR inputs, one for each channel.
10 cm is no problem for a buffered device.
These translators allow VCCA and VCCB to be the same. (You could also use a transceiver with a single VCC, or a plain buffer for unidirectional signals.)
The SIM data line is bidirectional, so it is not possible to use it with any '45 or '245 translator.
Clemens,
Thanks for the feedback. What you mean that we currently don't have the device that can be used for SIM data line right?
Best Regards,
Leroy Song