Part Number: TXS0108E
Other Parts Discussed in Thread: SN74AXC8T245
Hi
Problem description:
1. When the LTEVCC_EN signal in the circuit diagram turns on the 3904 transistor of Q68, the LTEVCC_EN signal will jump up and down due to insufficient drive capability
2. TXS0108ERGYR is a two-way Level shift IC, which causes the LTEVCC_EN_SOC of the input signal to be affected and jump up and down.
3. Then the PMU_PLTRST_N of different channels is also affected and cannot be pulled high normally, causing the board to fail to boot normally, and the OE signal is not affected
4. Q68 must be changed to 2N7002 transistor before it can return to normal
Questions:
I refer to the content of the datasheet, TXS0108ERGYR is an IC that is opened independently for each channel. Why does it affect the signals of different channels?