Part Number: SN74LVC1G123
Dear Specialists,
My customer is evaluating SN74LVC123 and encountering a problem.
I would be grateful if you could advise.
---
In SN74LVC1G123DCUR, one pulse signal of about 80ms is output from output terminal Q at 0.93V
on the way from Vcc = 0V to 5V.
(In the system, the circuit in the subsequent stage will operate due to the influence of the output signal.)
(1)Could you please let us know the cause of the phenomenon.
(2)We'd like to know how the risig and falling edge of the A, B and CLR determined.
Could you please see the waveform and schematic.
Question about SN74LVC1G123DCUR.xlsx
According to the Function Table, a pulse may be output when the IC_B or CLR transitions from L to H.
However, 0.93V is out of the operating rating.
We are looking forward to waiting your advice.
---
I appreciate your great help in advance.
Best regards,
Shinichi