This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXS0101: Need more details about OE pin

Part Number: TXS0101
Other Parts Discussed in Thread: TLV809E

Hi,

We have used TXS0101 in several circuit before without any issues. Usually, we connect OE to GND via a 100KOhm pull down, and connect it to the host that is powered by VCCA. The host then drives OE some times after booting up.

The problem:

Now, we have a circuit, where we need to do translation between 1.8V and 3.1V, and we don't have enough pins to drive OE. So I'm looking at my options.

What I intend to do is:

  • connect OE to 100KOhm pull down.
  • Connect OE to 1KOhm pull up to VCCA
  • Connect OE to open drains that keep OE low as long as both VCCA and VCCB are not stable 

Would that be enough?

If not, what exactly do i need to do with OE if I don't need to use it (and i don't have enough pins in my design to do so) ?

Thanks,