Other Parts Discussed in Thread: SN74AXC4T774, SN74LXC8T245-Q1
Hi Team,
We have the requirement of supporting Higher drive strength in one of the signal line at the output of translator.
In this case, If we use the part TXB0104, Please Confirm the below,
1) Whether we can short two Input pins (A1 & A2), & short two Output pins (B1 & B2).
(Note: For better understanding, Single Input signal will be provided to A1 & A2 & Single Output signal will be taken from B1 & B2).
2) If the above is correct,
(i) Really, can We achieve higher current output?
(ii) Whether this configuration will affect the speed/Data rate of the signal?
(iii) Is there any issues/Impacts in this configuration?
Thanks,
Ahamed Faize