Part Number: LSF0102
Other Parts Discussed in Thread: PCA9306, , TIGER
Hi,
Is there any graphic to show maximum speed V.S. load capacitance for 1.8V to 3.3V level shifter?
Currently, customer is using PCA9306 for 1MHz SMBus application, but it looks PCA9306 could only support up to 400KHz.
LSF0102 is p2p with PCA9306 in DQE package.
However, the maximum load capacitance may be up to more than 400pF, thus they want to check whether it is okay to run 1MHz at this kind of condition?
Please help!
Thanks and Best regards,
Tiger