Part Number: SN74LVC1G07
Hi Sir,
Are there any protection circuit for output pins within this device?
SN74LVC1G07DBVT is used at VCC + 3.3V in my schematic.
The pull-up resistance of the output pin side was mistaken for a 0 ohm resistor, and the output pin of pin4 and + 3.3V directly connected.
When the circuit was pull-up, the SN74LVC1G07DBVT was not broken and worked normally.
The Pin 2 input pin has a low level of + 3.3V power supply on to 2 milliseconds, and then has a high level of + 3.3 V.
Please confirm.
Thanks.
Regards,