Part Number: CD4046B
Other Parts Discussed in Thread: CD4022B
I am using CD4046B with octal counter cd4022b to to 44.1kHz-48kHz and ideally output locked x8 range. So far, best I can get is about 44.1kHz to 46kHz.
Can someone suggest changed values to widen usable input range for f_base?
Details:
I have the values as follows: C1=100pf (minimum allowed value) R1=20kOhms R2=100kOhms, R3=4.7kOhms C2=100pf. My goal here is to have a x8 output from the input (f_base) with an f_base of 44.1kHz-48kHz. My current selection of components allows me to have a range from about 43.9kHz-46kHz. Is there some way that I can widen the range a bit to extend it up to a little past 48kHz (just to give it some headroom for swings in f_base)?
Counter IC:
PLL IC:
ticsc.service-now.com/sys_attachment.do
Thanks