Other Parts Discussed in Thread: UCC27517
Hello team,
Our customer would like to drive Nch FET from output SN74LVC1G02 directly.
Here is the specification.
- Power supply 5V
- SW frequency 100kHz
- FET
- Ciss 1.4nF
- Gate resistor 1.3ohm
- VGS 1.0V – 2.0V
They estimate max output current from gate of FET to output of logic will be 5V / 17ohm = 294mA since the output impedance of logic could be calculated ROH = 22ohm and ROL = 17ohm.
The time flowing current at 294mA will be around 5u sec.
I believe the above operation is over absolute maximum ratings, so cannot be acceptable.
If you have any proposal, please let me know.
Thank you and best regards,
Michiaki