This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXB0104: Whether it is suitable product for my customer requirement?

Part Number: TXB0104


Dear Teams,

My customer has following requirement:

IC Type: Buffer IC; Used to voltage level shift between 3.3V and 5V

Channel: 4 channel, one of channel is reverse direction

Isolation: Non-isolation

Communication: Used for SPI communication

Based on above requirement, I choose TXB0104 to promote. Do you think it is best product to promote based on customer requirement? Do you have any suggestions?

Thanks!

Dylan