Hi team,
I want to check if the pull up/down resistor can be placed at input I/O port of SN74AXC4T245-Q1 (1.8V to 3.3V). This is because a slave deivce has a shared port (Mute/Address pin). At the power up sequence of the slave device(3.3V), the high or low will determine the device address. And then, the port is used as Mute pin through AP control. So, is it possible to use pull up/down resistor together at the I/O port?
Thanks,
Sam Lee