Part Number: TXS0108E
Other Parts Discussed in Thread: SN74AHC541, SN74AHC125
Hi Team!
Currently we are designing our PCB with the TXS0108E. As we also have some external limit switches with 5V supply voltage, we would like to connect them to our 3V3 MCU via the level shifter. Therefore we tested it with a 1M Pull-Down resistor on one of the B input pins and also with 5V supply voltage. Unfortunately we were not able to get the desired output level while changing from no input voltage (GND via Pull-Down) to 5V. We also have a question regarding the OE input pin: Is it necessary to also have there a Pull-Down resistor or can it directly be connected to the A port voltage level of 3V3? We also noticed that there might be an issue with the Pull-Down resistor value at the signal input pin if it is too low but we think we chose it high enough. Attached is the schematics. Thanks in advance.