Part Number: CD14538B
Other Parts Discussed in Thread: SN74LVC1G123
Hi, expert,
Do you have CD14538 function table? and what's the updated device with the same function as this device? Thanks.
Best Regards
Chen
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CD14538B
Other Parts Discussed in Thread: SN74LVC1G123
Hi, expert,
Do you have CD14538 function table? and what's the updated device with the same function as this device? Thanks.
Best Regards
Chen
Hi Chen,
There isn't a function table for this device, but it's operation is relatively simple. The CD14538B contains two independent retriggerable monostable multivibrators.
When triggered, the device will output a pulse of a fixed width (determined by the timing components Rx and Cx). Because the device is 'retriggerable,' the device can be triggered again while the output pulse is occurring, and it will cause the output to extend.
The device can be triggered with a rising edge via the +TR input or a falling edge with the -TR input. There is also a clear input that allows for interrupting the output pulse to reset the device.
The device also includes an inverted output, which is just the opposite of the primary (Q) output.
There are other monostable multivibrators in our portfolio (see Monostable Multivibrators), however this device doesn't have a newer version.
Hi, Emrys
Thanks for your reply, It's clear that the basic work principle of this device. May I understand that CD14528B has the same function table with SN74LVC1G123?
Best Regards
Chen
Hey Chen,
No, they aren't the same, although they both are retriggerable monostable multivibrators.
The CLR\ pin of the CD14528B is only indicated for resetting the device and doesn't trigger the output on release like the SN74LVC1G123. Also, the CD14528B has an inverted output while the SN74LVC1G123 does not.
It might be helpful if you told me what you were trying to do -- do you need a monostable multivibrator with a particular function set?