This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC2G38: Level shifter

Part Number: SN74LVC2G38
Other Parts Discussed in Thread: SN74LVC1G38

Hi,

I would like to use the SN74LVC2G38 as a level shifter. The voltage supply is 1.8V and the output should pull down a 3.3V load to GND. I think this does not work becuase the output is limited to VCC. The SN74LVC1G38 should fit because the output is specified up to 5.5V and not limited to VCC, correct?

Thanks a lot!

Best regards, Xaver