This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXS0108E: Can i use a 5V signal to trigger the output enable?

Part Number: TXS0108E


Hi team,

If I have both VCCA and VCCB on the TXS0108 part set at 3.3V, can I use a 5V signal to trigger the output enable or should I voltage divide that signal down?

Thanks,

Kevin 

  • Hi Kevin,

    The info you're looking for is described in the recommended operating conditions table of the datasheet here:

    As indicated above, for the OE pin, any input value above VCCA * 0.65 and less than 5.5V is considered a recommended input -- so 5V is perfectly fine.