Part Number: SN74HCS365
Hi Team,
According to datasheet Maximum Icc is 2 µA.
The customer is using it on 3.3V, the current of bare chip test has 50 ~ 200µA fluctuation, and 3mA under 6V.
Even if it is not connected to OE and IO, and only connected to the power supply pin, the power consumption is still very high.
What are the test conditions for 2 µA?
Is it according to Figure 6-3 and Figure 6-4 on datasheet?
Beat Regards,
Tom Liu