e2e,
I'm using SN74LVC16244 in switch product for signal hotswap purpose.
There are two separate boards, Board A and Board B has connection from SN74LVC16244.(two board has some ground)
A board, output is high, and B board’s power VDD3.3V_B drop, we can see VDD3.3V_B has 0.75V to ground, and A board’s input pin is clamp to low.
A board output pin is low when B board power VDD3.3V_B drop, then A board pin are normal, VDD3.3V_B is normal 0V, and A board’s input pin is high.
Could you please help analyze when A board is active and B board is power loss, how to impact SN74LVC16244’s behavior? Thanks.
Adam