Other Parts Discussed in Thread: LSF0102
Hi
When I looked for a solution for RMII & MDIO level shift, I got confused about SN74AXCH8T245RHLR and TXB0102DCUTG4.
The datasheet of TXB0102DCUTG4 shows it cannot use strong pull high or down resistor, because of the drive resistor is 4K Ohm.
Is there the same "note" in SN74AXCH8T245RHLR?
Because my RMII signals have the strap function and the recommended pull up/down resistors are 4.7K~10K, I don't know if I can use SN74AXCH8T245RHLR or not?
The MDIO signal is bi-directional, and the minimum rate is 20MHz. The switch chip also shows needs pull up resistor and 10K Ohm.
Could you help to find the component?
Thanks