This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXS0102: Need High Speed Suggestion of TXS0102DCU

Part Number: TXS0102
Other Parts Discussed in Thread: LSF0102

Hi Sirs,

Would you pls provide a high speed version of TBS0102? The current device support 4.8MHz clock while my customers needs 9.6MHz for MDIO.

Thank you and Best regards,

Wayne Chen
02/04/2021

  • Hey Wayne,

    There is no "high speed version" of that device. You can use the LSF0102 device which can operate at higher frequencies, but it will ultimately depend on the pull-up resistor sizes and interfacing devices drive strength. Here are a series of training videos that will help you understand the LSF family. In these videos you will see how to properly bias the device and how to size the pull-ups appropriately for the data rate.