Part Number: SN74LVC8T245
Hello
Please tell me if the latch-up test current is "± 100mA".
Thanks
Best regards,
Masahiro Kobayashi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN74LVC8T245
Hello
Please tell me if the latch-up test current is "± 100mA".
Thanks
Best regards,
Masahiro Kobayashi
Masahiro Kobayashi,
As the datasheet states this devices 'Latch-Up Performance Exceeds 100 mA Per JESD 78, Class II'
Thanks,
Rami Mooti
Hi Rami,
Thank you for your response.
Is the latch-up test current done at -100mA in adeition to 100mA?
Thank you.
Best regards,
Masahiro Kobayashi
Kobayashi-san,
Yes the latchup immunity will cover the -100mA and +100mA injection scenarios.
Thanks,
Rami