Part Number: SN74LS2323
Other Parts Discussed in Thread: TLV713
Provide case details or comments: My concern is that when I use a number of these parts (lets say 5 on one design), I typically bias the reference pin with one common connection to a voltage divider. This would be for A 5V power supply operation, I would usually use a voltage divider, 5V to 1k ohm to 665 ohms to GND, then pick off the voltage at the 665 ohm resistor which is ~2V for the reference. The common strobe is always tied to GND (so part is enabled)
My question is, how much current does the reference input (pin #6) need, is the network I described sufficiently low impedance to bias all five in parallel? What would be a safe bias network to bias 5 parts from a common reference, is a voltage reference needed or is a resistive voltage divider sufficient?