Part Number: TXS0108E
Other Parts Discussed in Thread: TXB0108, SN74AXC2T245, SN74AXC8T245, SN74AXC4T245
Hi team,
Does TXS0108E support UART level conversion?
BR
Gust
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TXS0108E
Other Parts Discussed in Thread: TXB0108, SN74AXC2T245, SN74AXC8T245, SN74AXC4T245
Hi team,
Does TXS0108E support UART level conversion?
BR
Gust
Yes. For an UART alone, [FAQ] Are there voltage level translation / level shifter device recommendations for the industry standard interfaces like GPIO, SPI, UART, I2C, MDIO, RGMII, I2S etc? recommends other devices, but the TXS also supports this.
Hi Clemens
Thanks for your reply. TXB0108 can support UART level conversion, right? I want to convert 1,8V to 3.3V
BR
Gust
The TXB has many restrictions on the input and output signals, but it can support UART.
Hey Gust,
I recommend the SN74AXC2T245 (2 ch), SN74AXC4T245 (4 ch), or SN74AXC8T245 ( 8 ch). Each one of these devices can support UART.
Hi Dylan,
Thank you for your help. Do three chip support 1.8V convert 3.3V?
BR
Gust
Hi Gust,
Yes, the above three devices support translation from 3.3V to 1.8V and vice-versa.
Thanks!
Chad Crosby