Other Parts Discussed in Thread: TXB0102, SN74LVC1G17, SN74LVC1T45
Hi Team,
Our customer is using TXS0102 in their system for UART signal translation(5V to 1.8V), due to their TX side circuit limitation, there is 2K resistor in serial on the TXD line as show in below schematic, thus it will cause a very high VOL when TXD output "L". Without changing their solution, they want to add a 20K resistor in serial on VCCB node which will decrease VOL to around 500mV which should meet their specification, so they want to check if we can use TXS0102 like this method - can you help to check it?
Original circuit:
Modified circuit:
Also, it looks like TXB0102 will have no such issue, but we don't find DCT package customer currently used for TXS0102, can you also help to check if we have TXB0102DCTR or TXB0102DCTT samples available now?
Thanks.