Part Number: SN74HC4060
Hi Team, posting for a customer, I hope you can help us clarify this.
Looking for is TI documentation for the two chips the 74HC4060 and the 74HC40103 which explains them in the same way. No documentation, figures out the clock cycles and the input frequency to figure out which pin they need to tap to get the division they need, the just look at something similar to what I provide and say, for example, I have a 4mHz signal coming in and if I want a 250 kHz signal out, they can use a 74HC4060 and use pin 7 to divide by 16.
Hoping for your inputs.
Regards,
Mark