This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AHC1G00: Will the output at high when Vcc drops?

Part Number: SN74AHC1G00

Hi

I'm using the 2 input NAND of SN74AHC1G00 with 3.3V of Vcc.

The input A is powered by a pull-up resistor to 3.3V while the input B is connected directly to 3.3V.

What I want to know is that if Vcc slowly drops from 3.3V, will the output be at high?

My understanding from the datasheet is that since VIH=Vcc×0.7, the output will not be high when Vcc drops, is that correct?

Thanks

David H.