This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC2G07: VIH when VCC=2V?

Part Number: SN74LVC2G07


Hi guys,

Working with a customer on this. We are using the SN74LVC2G07DBVR and in the application, VCC = 2.0V, and the expected VIH  = 1.75V. Reading the datasheet, the VCC falls in-between the ranges, what is the VIH threshold at VCC=2V?

Should it be VCC*0.65?

Thanks in advance!