This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LSF0108: Communication issue + schematic review

Part Number: LSF0108
Other Parts Discussed in Thread: SN74LVC1T45

Hi,

I am implementing a new sensor (supply voltage is 1.8V) that uses I2C interface, and our host MCU is using 3.3V.

Besides the I2C (SDA, SCL), this sensor also has the following pins:-

1 x open-drain (RST)

2 x push-pull (PROG, DIR)

1 x INT (direction control is required)

For this application, I am using LSF0108 + SN74LVC2T45DCTR.

So far, I am not able to get successful communication and not sure what went wrong.

Attached is the connection diagram, can you please review it and let me know if you have any recommendations?