Hi Team
Could you tell us ESD(HBM) spec of the following items?
1:SN74LS32DBR
【ESD Spec:Example】
Best regards'
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team
Could you tell us ESD(HBM) spec of the following items?
1:SN74LS32DBR
【ESD Spec:Example】
Best regards'
Hi,
Unfortunately, we don't have this information readily available - as this is an older part. If you'd like, I can check to see if we can test this part, but the ESD testing may take anywhere from 1 to 2 months to do. Would you like for me to check this for you?
Thanks!
Chad Crosby
Hi Chad Crosby-san,
Thank you for your support.
I understand that there is no information about ESD of SN74LS32DBR.
So, are there any products that have already been ESD tested in the same series and in the same package that can be shown to have the same ESD (HDM)?
Best regards'
Akio Minami
Hi Minami-san,
I was able to find a test for the SN74LS123DR and it passed the following:
| ESD HBM | 2500V |
| ESD CDM | 1500V |
| ESD MM | 250V |
This is likely the case for the SN74LS32, as both are bipolar devices. There should be minimal to no variations for ESD performance between different packages.
Thanks!
Chad Crosby