This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Graphics display driver which supports touch-sensitive LCDs and compatible display



Hello,

I'm looking for a Graphics display driver which supports touch-sensitive LCDs and also a compatible display with the following requirements: 

Max display size= 5"

VDD max= 5V

required current max = 1A

The interface can be both I2C or SPI. 

If the driver comes with a EVKIT would be great.

I have quickly looked at the TI LCD drivers, but I don't understand what other equipment I have to use to complete my GUI project.

Thank you