This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AS869: Need equivalent part

Part Number: SN74AS869


I have used "SN74AS869DW" part in our existing design to generate 7.813KHz, 1MHz, 32MHz, 16MHz and 8MHz clock and it will support 5V logic only. 

Now, I need a counter to generate the same clocks. But, It have to support 3.3V and 5V logic. Can you please suggest the suitable part number for this requirement?