Other Parts Discussed in Thread: SN74LXC8T245, SN74LVC1G34
Hi Team,
Our customer is using TXB0108 with VCCA of 1.8V and VCCB of 3.3V. Section 6.3 of the datasheet shows that the maximum voltage of VIH is VCCI. However, our customer would like to confirm if the inputs at VCCB port are 5V tolerant. If not, can they use voltage divider before VCCB port to reduce the voltage from 5V to 3.3V? If this is a possible, can you please suggest the values of the resistors for the voltage divider?
Regards,
Danilo