Other Parts Discussed in Thread: SN74CB3T3306
as for SN74CB3T3306, the datasheet shows that: Absolute Maximum Ratings: VCC Supply voltage range(2) –0.5~ 7 V Recommended Operating Conditions: VCC Supply voltage 2.3 ~3.6 V Why do the two reatings have so big difference? and we want 5V output, so we connect the VCC to 5V power. Is it OK? does the electric charactors such as Ron, tpz will change if we use the chip out of range of the Recommended Operating Conditions?