I am trying to repair a fan controller board that is part of a VPX development chassis I own. The bad component is a TI part NH245 which appears to be a variant of the SN74LVC8T245; this is the part that shows up when I search for NH245. However the NH245 part appears to support B port voltages of 12V whereas the standard part is only capable of supporting 5V. I am trying to obtain replacement parts for the NH245. Can you provide me with details on how I can procure the NH245 part.