This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXB0104: The data I/Os of TXB0104 must have drive strength of at least ±2mA. How figure the 2mA out?

Part Number: TXB0104


The data I/Os of TXB0104 must have drive strength of at least ±2mA. How figure the 2mA out?

  • This input drive strength isn't a specification defined by the TXB0104 device. ±2mA is the minimum drive strength recommended for the device that is actually driving the data I/O pins. You can usually find this in the datasheet or manual of the controller you're using to drive these signals.

    Thanks,
    Rami