This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LV14A: what is the input transition rate of SN74LV14A?

Part Number: SN74LV14A
Other Parts Discussed in Thread: SN74LV540A

Hi Team 

My customer wants to know the input transition rate of SN74LV14A. It is not shown in datasheet. 

I found following material showing LV family have 100ns/V(max) input transition rate.

https://www.ti.com/lit/wp/slla364a/slla364a.pdf#page=2

Is this still true for SN74LV14A? I am asking because it has schmitt trigger, customer wonders if there's any difference for input transition rate with and without schmitt trigger.

For example, SN74LV540A, which have no schmitt trigger, shows 100ns/V input transition rate at Vcc=3V to 3.6V condition. 

Thanks.

Regards,

Jo