This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LV1T125: Connect two SN74LV1T125 to level translate from 1.8V to 5V

Part Number: SN74LV1T125
Other Parts Discussed in Thread: SN74LVC2T45, SN74AHC1G125, TXS0101, TXB0101

Hi Team,

Our customer is looking for a single +1.8V to +5V unidirectional voltage translator with tristate output. I have checked our product lines but it seems we don't have this type of device.

Can we connect two SN74LV1T125 such that the output of the first device goes to the input of the second. Then the VCC of the first one will be connected to a 3.3V supply and will translate the voltage from 1.8V to 3.3V while the VCC of the second one will be connected to 5V supply and will translate 3.3V to 5V. Please refer to the diagram below. Is this feasible?

Regards,

Danilo