Hi
I am using this part LSF0204D for a UART interface (push-pull ) from a SOM from Nvidia JTX1 1.8V to ELM chip 5V side .
In the 1.8 V side since it is push pull i have not used any pull up do we need to use pull up on both sides ?
I am using this part TXB0304RSV for a SPI interface (push-pull ) from a SOM from Nvidia JTX1 1.8V to ISP chip 3.3v side .
In the 1.8 V side since it is push pull i have not used any pull up do we need to use pull up on both sides ?
can i use this part LSF0204D for both UART and SPI instead of two separate part ?
SPI max clock from processor is 65Mbps clock 65Mhz
UART from processor 12.5Mbps baurd rate