Part Number: SN74LVC573A
Hello,
is the SN74LVC574ARGYR qualified for Ta -40°C to 125°C ?
On page 2 in the datasheet -40°C ..85°C is specified for VQFN20 package (this is the RGY type)
On abbendum page 2 the datasheet specifies -40°C to 125°C for the SN74LVC574ARGYR.
What is correct? what parameters in this datasheet are valid for the SN74LVC574ARGYR?
thanks
Ronny