This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] Why does a logic device's part number have an E4/G4 suffix?



FAQ: Logic and Voltage Translation > Quality and Manufacturing >> Current FAQ

In short, there will be no difference between a device labelled SN74xxG4 and SN74xx.

Historically, G4 and E4 suffixes meant that the devices were rated to be "Green" or "Lead Free." However, as time has passed, all devices have been pushed to these new "Green" or "Lead Free" standards, but the part numbers have remained available so that customers have had a consistent orderable part number.

E4 – Pre-plated, NiPdAu

June 2004, TI defined ‘Green’ mold compound as:   Br or Sb < 0.1% by homogeneous weight

G4 – meant pre-plated with ‘Green’ mold compound

To check on the "Green" status of a part, you can put your part number into the search at the following link:

Material Content Search Tool

For definitions of E4, G4 suffixes, please refer to the following:

Environmental Information

Environmentally Friendly Solutions from TI

You can also refer to the end of the datasheet in the Part Orderable Addendum to see the "Eco Plan" of a specific part orderable.

The electrical specifications for every device listed in the orderable addendum is that listed in the datasheet.