This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] How does a slow or floating input affect a CMOS device?

Guru 60600 points

Replies: 0

Views: 3269

FAQ: Logic and Voltage Translation > Input Parameters >> Current FAQ

There are two primary issues associated with slow and floating inputs.

Not sure what a 'floating input' is? Please see our FAQ: What is a floating input or floating node?

(1) Shoot-through current

Figure 1. Typical CMOS input structure with the control voltage for each input MOSFET shown.

CMOS logic devices depend on their inputs being at either a logic HIGH or a logic LOW. 

When the input is 'somewhere in the middle,' then it's easy to see from Figure 1 that both MOSFETs on the input can be turned on, which can cause a significant amount of shoot-through current. It is best to transition through this voltage region as quickly as possible to prevent shoot-through current.

(2) Oscillation

(Thanks to  for this image)

When the input lingers near the threshold value (typically 1/2*Vcc) then the output can oscillate between the LOW and HIGH state uncontrollably.

For any CMOS device that does not have Schmitt-trigger inputs, the datasheet defines a minimum input transition rate that will prevent this from happening.

For more information, see the application report Implications of Slow or Floating CMOS Inputs


Looking for a low voltage translator? Check out the AXC family that supports 0.7V to 3.3V translation!

The Logic Minute training page has videos on many interesting topics that all are kept shorter than 5 minutes.