Other Parts Discussed in Thread: SN74AHC540, SN74AHC16540, SN74AHC240
Hi,
I am looking for a chip which would act like a "NOT Gate".
Requirement is: I have two select lines wherein i want to select either of the 1 between 2. So when 1 pin drives to VCC other would drive to 0V. It would be good if a chip has array of NOT Gates. High on line-> 2V to VCC. VCC i am good with 3.3V - 5V.
Please suggest suitable part for this.