Part Number: SN74LV221A
Other Parts Discussed in Thread: CD74HCT221
Hello
We have a product using the SN74HCT221A and evaluating whether the SN74LV221A will be a drop in replacement.
This thread describes a difference in the LV part:
SN74LV221A: SN74LV221A Shorter pulse than expected on output
Our circuit has a 510R and 200pF RC LPF then an VHCT125 buffer prior to the HCT221A inputs. The RC has been noted as a revision to remove input noise. Our input circuit is being changed and I am wanting to also delete the RC LPF and VHCT125.
Has TI evaluation from the thread above determined that the re-triggering issue is present only on the LV part ?
Also, has examination confirmed that the re-triggering failure only occurs during the capacitor discharge period as Nicolas' tests indicate ?
We have a 3.3 volt supply, Ct 470pF and Rt 1k (for 630nS output pulses) and our slow rise-times on a new opto-isolator at the inputs are unlikely to let through pulses as Nicolas demonstrated.
Thank you
Harry