This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Draining of RTC battery (Lithium coin battery) in the off condition.



Hi,

I used a Lithium coin battery (part number BR-2330/HEN) as a back up voltage for RTC chip (part number DS1307). The board works normal. But after storing  a number of boards for around 1 month, the RTC battery got drained off (from 3V to 0.5 or 0.3V). I replaced the battery after which the RTC functionality works normal.

What may be the reason for draining of the battery? The current capacity of the battery is 255mAh. As per the datasheet the leakage current through the  RTC chip backup voltage pin is in nano amps range. I don't find any path for the discharge. And this is the battery recommended for the RTC chip mentioned here. 

Please drop your comments/suggestions/observations about this issue.

Thank You,

Vijetha H.N