Other Parts Discussed in Thread: TXS0102, TXB0102
Hi There,
I will be using the TXS0102 device for voltage translation between 1.8 VDC (VCCA pin) and 5 VDC (VCCB pin) UART signals.
My question relates to the OE pin. For the TXB0102 device, that data sheet mentions that the OE pin is just connected to VCCA internally. For the TXS0102 device, the data sheet only talks about connecting the OE pin to ground when the device is not needed.
Assuming that the OE pin for the TXS0102 device needs to be connected to the VCCA pin, should I put a 10k resistor between OE and VCCA?
I searched online for an example and this design did that, but I wanted to be certain this resistor is needed.
http://omer.me/uploads/ponte-schematic-revc-300x197.png
Oh, and I understand that I could just use the TXB0102 device, but I already have the symbol/layout for the TXS0102.
Many thanks,
James